SNOSDB6D December 2020 – October 2024 LMP7704-SP
PRODUCTION DATA
The LMP7704-SP can be used as a precision current source in many different applications. Figure 6-6 shows a typical precision current source. This circuit implements a precision, voltage-controlled current source. Amplifier A1 is a differential amplifier that uses the voltage drop across RS as the feedback signal. Amplifier A2 is a buffer that eliminates the error current from the load side of the RS resistor. In general, the circuit is stable as long as the closed-loop bandwidth of amplifier A2 is greater then the closed-loop bandwidth of amplifier A1. If A1 and A2 are the same type of amplifiers, then the feedback around A1 reduces bandwidth compared to A2.
The equation for output current is derived as shown in Equation 4:
Solving for current I results in Equation 5: