SNOSDL9 December 2024 LMG5126
ADVANCE INFORMATION
The output capacitors smooth the output voltage ripple and provide a source of charge during load transient conditions.
Ripple current rating of output capacitor must be carefully selected. In boost regulator, the output is supplied by discontinuous current and the ripple current requirement is usually high. In practice, the ripple current requirement can be dramatically reduced by placing high-quality ceramic capacitors earlier than the bulk aluminum capacitors close to the power switches.
The output voltage ripple is dominated by ESR of the output capacitors. Paralleling output capacitor is a good choice to minimize effective ESR and split the output ripple current into capacitors.
The single phase boost output RMS ripple current can be expressed as:
The output RMS current is reduced with interleaving as shown in Figure 7-4. Dual phase interleaved boost output RMS ripple current can be expressed as:
Decoupling capacitors are critical for minimized voltage spike of the MOSFETs. This is also important from EMI view. Quite a few 0603/100nF ceramic capacitors are placed close to the MOSFETs following "vertical loop" concept. Refer to Improve High-Current DC/DC Regulator EMI Performance for Free With Optimized Power Stage Layout application brief for more details.
A few 10µF ceramic capacitors are also necessary to reduce the output voltage ripple and split the output ripple current.
Typically, aluminum capacitors are required for high capacitance. In this example, four 150µF aluminum capacitors are selected.
The output transient response is closely related to the bandwidth of the loop gain and the output capacitance. According to How to Determine Bandwidth from the Transient-response Measurement technical article, the overshoot or undershoot Vp can be estimated as:
where ΔItran is the transient load current step.
Please be aware that Equation 27 is valid only if the converter is always operating in CCM or FPWM during load step. If the converter enters DCM or pulsing skip mode at light load, the overshoot is worse.
Due to the inherent path from input to output, unlimited inrush current can flow when the input voltage rises quickly and charges the output capacitor. The slew rate of input voltage rising must be controlled by a hot-swap or by starting the input power supply softly for the inrush current not to damage the inductor, sense resistor or high-side MOSFET.