SNOU170A August   2020  – December 2020

 

  1.   Trademarks
  2. 1Introduction
  3. 2Features
  4. 3EVM Specifications
  5. 4Recommended Equipment
  6. 5Quick Start Procedure
  7. 6Board Setup
    1. 6.1 Supply Voltage
    2. 6.2 Inputs
    3. 6.3 Outputs
  8. 7Layout Guidelines
  9. 8Schematic
  10. 9Bill of Materials

Quick Start Procedure

Note: DO NOT TURN ON POWER SUPPLY UNTIL ALL CONNECTIONS TO THE DEVICE ARE MADE TO THE BOARD.
  1. Set VCCI/VCCO Power Supply to 3.3V and disable the power supply output
  2. Connect positive terminal supply to TP5, and negative terminal to TP4
  3. Ensure that cables connecting to IN+, IN-, IN+SENSE, IN-SENSE, OUT+, and OUT- are matched length and impedance. Perform any deskewing if necessary.
  4. Set the function generator to produce a square wave output with 100mVpp at 50MHz, with a DC offset of 1.65V. Disable the signal generator output. Connect the output to IN+.
  5. If available, use the second channel on the function generator to create a complementary signal to the one created in step 3. Disable the signal generator output. Connect the output to IN-.
  6. If a second channel or another function generator is not available, use a power supply set to 1.65V. Disable the output and connect to IN-. An adapter to connect the SMA connector on the board may be needed.
  7. Connect OUTP and OUTN to a 50Ω terminated scope. Alternatively, use a differential probe with a 100Ω termination and connect to the oscilloscope.
  8. Connect IN+SENSE and IN-SENSE to a 50Ω terminated scope channel.
  9. Enable the power supply and the signal generator.
  10. Verify the supply current is < 17.5mA
  11. Monitor and verify the inputs from IN+SENSE and IN-SENSE
  12. Monitor and verify the outputs for OUT+ and OUT-
GUID-20200803-CA0I-KH39-168F-DFFWPWFN0XDZ-low.pngFigure 5-1 TLV3604 EVM Quick Start Setup
Next is a scopeshot capture of the inputs and outputs described in the quick start procedure. Here, the propagation delay between IN+ and OUTP/OUTN is measured by taking the time delta between when IN+ and IN- cross, and when OUT+ and OUT- cross. The low to high propagation delay in the figure below was calculated to be 682 ps.
GUID-20200803-CA0I-M8HG-TJZ8-2NSNQSXSJFHW-low.pngFigure 5-2 Quick Start Example.