SNOU183 May   2021 TLV3601 , TLV3601-Q1 , TLV3603 , TLV3603-Q1

 

  1.   Trademarks
  2. 1Introduction
  3. 2Features
  4. 3EVM Specifications
  5. 4Recommended Equipment
  6. 5Quick Start Procedure
  7. 6Board Setup
    1. 6.1 Supply Voltage
    2. 6.2 Inputs
    3. 6.3 Outputs
    4. 6.4 Hysteresis
  8. 7Layout Guidelines
  9. 8Schematic
  10. 9Bill of Materials

Quick Start Procedure

CAUTION: DO NOT TURN ON POWER SUPPLY UNTIL ALL CONNECTIONS TO THE DEVICE ARE MADE TO THE BOARD.

The following connections are made using a split supply configuration. Split supply configuration is advantageous for measurement purposes. The reference voltage can be set to GND, while the other input can be set to an AC waveform that toggles between negative and positive voltage at a 0 DC offset. Thus, the output will be toggling whenever the AC waveform toggles.

This configuration allows for 2 distinct advantages compared to a single supply input. The first advantage is that the reference voltage is at GND; a non-noisy voltage level. If the reference voltage level needs to be changed in relation to the supplies, the supply voltages can be altered instead. The second advantage being able to zoom into the input as much as possible due to the 0 DC offset of the waveform.

  1. Set power supply positive terminal to 2.5 V and negative terminal to -2.5 V. Disable power supply output.
  2. Connect positive terminal supply to TP1, negative terminal to TP2, and GND to TP3.
  3. Ensure that cables connecting to IN+SENSE and OUT are matched length and impedance. Perform any deskewing if necessary.
  4. Set the function generator to produce a square wave output with 100mVpp at 1 MHz, with a DC offset of 0 V. Disable the signal generator output. Connect the output to IN+.
  5. Connect IN- to GND through an SMA 50 Ω termination barrel.
  6. Connect OUT to a 50Ω terminated scope channel.
  7. Connect IN+SENSE to a 50Ω terminated scope channel.
  8. Enable the power supply and the signal generator.
  9. Verify the supply current is < 60 mA.
  10. Monitor and verify the input from IN+SENSE.
  11. Monitor and verify OUT.
GUID-20210420-CA0I-BR26-NNVD-LHLRQ1TK77HN-low.svg Figure 5-1 TLV3601 EVM Quick Start Setup

Next is a screen capture of the inputs and outputs described in the quick start procedure. Here, the propagation delay between IN+ and OUT is measured by taking the time delta between when IN+ and OUT reach 50% of their respective transitions. The low to high propagation delay in Figure 5-2 was calculated to be 2.184 ns while the high to low propagation delay in Figure 5-3 was measured to be 2.155 ns.

GUID-20210419-CA0I-NL7L-BQG4-TT87XXZFRG2B-low.svg Figure 5-2 Propagation Delay Rise Portion
GUID-20210419-CA0I-LZ5W-KJLT-RTZ55CMN893H-low.svg Figure 5-3 Propagation Delay Fall Portion