SNOU187 September 2021
By default, the TVS diode D2 at the input is not populated as the LM74721-Q1 enables input TVS less system designs for automotive ISO7637-2 pulse 1 suppression. A suitable TVS can be populated in case voltage transients beyond the absolute maximum rating of the device can occur on the positive side in the system.