SNOU204 October 2024
Q1 is a MMBT3904LP NPN BJT. This is used as the remote temperature sensor on the EVM. The MMBT3904LP typically has an N-factor of about 1.0042. The TMP9R01 assumes an N-Factor of 1.008, which can cause a temperature error in the remote temperature reading. The GUI automatically sets the N-Factor correction register to 1.0042 to compensate for this. If the device is reset, then the device sets the N-Factor correction register back to the default value or 1.008 and a temperature error can be seen. If a remote temperature error is seen, then use the N-Factor correction feature to adjust the temperature reading. The MMBT3904LP can also be broken off to allow the engineer to connect a different temperature remote to the device.