SNVA559C September 2012 – February 2019 LM2574 , LM2575-N , LM2575HV , LM2576 , LM2576HV , LM2577
The LM2577 is an IC developed as part of the SIMPLE SWITCHER® product family. It is a current-mode control switching regulator, with a built-in NPN switch rated for 3-A switch current and 65-V breakdown voltage.
The most commonly used applications are for Flyback or Boost regulators (see Figure 25). In the Boost regulator, the output is always greater than the input. In the Flyback, the output may be greater than, less than, or equal to the input voltage.
The theory of operation of the flyback and boost converters has been previously covered, and will not be repeated here.
The LM2577 is targeted for applications with load power requirements up to a maximum of about 25 Watts, and can be used to implement boost or flyback regulators (with multiple output voltages available if flyback is selected).
The next sections will show the LM2577 being used in circuits which are more advanced than the typical applications (these circuits were generated as solutions for specific customer requirements).