The purpose of this application note is to lead the reader through the design of an isolated buck also known as a Fly-Buck™ converter using the LMR36520 from Texas Instruments. This application note will describe the typical operation of a Fly-Buck™ converter from a theoretical perspective, and then walk through the process of Fly-Buck™ converter design from a set of given operating conditions using design equations derived in referenced reports. Physical measurements will be compared to expected results, and design limitations will also be discussed.
Fly-Buck™ is a trademark of Texas Instruments.
SIMPLE SWITCHER® is a registered trademark of Texas Instruments.
All trademarks are the property of their respective owners.
Many applications require various power rails to supply power to different devices within a system. It is not uncommon for these different power rails to each have differing load requirements. Some rails may need to be very tightly regulated, offering a minimum of peak-to-peak variation to meet their respective load requirement. Some rails on the other hand, can power loads that are more robust to variations on the input supply and, therefore, do not require such tight regulation.
Rather than having a different DC/DC regulator for each different power line, some systems can benefit from using a single IC to produce multiple power rails. The Flyback topology offers the possibility of producing multiple power lines from a single input, but that comes with a cost of using more complex control circuitry to regulate the secondary. This is where the isolated buck, or Fly-Buck™ converter, comes in. The Fly-Buck™ converter is a modification to the standard buck converter topology that replaces the standard inductor with a coupled inductor or transformer to produce one or multiple isolated secondary outputs.
The Fly-Buck™ converter topology is beneficial because it produces a tightly regulated primary output, along with one or multiple electrically isolated secondary outputs without the need of using an optocoupler to regulate the secondary. This means that the design of a Fly-Buck™ converter is relatively straight forward and can be done similarly to the design of a typical buck converter with some minor variations.
This application note will detail the process of designing a Fly-Buck™ converter using the LMR36520. The LMR36520 is a 4.2-V to 65-V 2-A synchronous buck converter that is well-suited for industrial power applications. The HSOIC-8 package can handle PCB strain better than other leadless packages and also makes debugging in the field much easier by enabling visual inspection of the device leads. Internal compensation reduces external component count and simplifies pinout making the LMR36520 ideal for Fly-Buck™ converter applications.