When selecting a optocoupler a few major parameters need to be considered: current transfer ratio (CTR), diode voltage drop on the secondary side, and the capacitance of the BJT on the primary side. In the following equations CTR is synonymous with kOPTO, the diode drop with VD and the BJT capacitance with COPTO in Figure 3-2.
- The CTR varies drastically based on the selected component. There can be as large as 600% variance in the CTR value over operating conditions. Due to this large tolerance in CTR, the loop compensation component selection needs to account for the minimum CTR value and maximum CTR value. In this design the CTR of the selected optocoupler is 100% to 200%.
- The diode voltage drop impacts the selection of the RLED value. The diode drop need to be small enough to allow the voltage reference to be supplied with adequate voltage to ensure operation. The diode drop of the selected optocoupler is 1.4V.
- The pull-up resistor (RPULLUP) and the parasitic capacitance
(COPTO) form a pole, limiting the maximum crossover frequency of
the control loop. Once the pull-up resistor is selected the capacitance of the
optocoupler is calculated from the optocoupler data sheet. The selected
optocoupler the capacitance is calculated to be approximately 3.3nF. The cross
over frequency should be less than the pole, which is roughly 9.66kHz for this
design.
Table 3-2 summarizes the key parameters of the selected optocoupler.
Table 3-2 Selected Optocoupler
parameters
Parameter |
Value |
kOPTO_min |
100% |
kOPTO_max |
200% |
VD |
1.4V |
COPTO |
3.3nF |
VCE(sat) |
200mV |