SNVA866A February 2019 – January 2023 LM5155 , LM5155-Q1 , LM51551 , LM51551-Q1
The external under voltage lockout (UVLO) resistors set the minimum operating supply voltage of the regulator. Two levels must be specified; the voltage the LM5155 starts operation (VSUPPLY(ON)) and the voltage the LM5155 enters stand-by mode (VSUPPLY(OFF)). In this example, VSUPPLY(ON) voltage is 17 V and the VSUPPLY(OFF) is 16 V. Using Equation 24, the top UVLO resistor (RUVLOT) is calculated.
RUVLOT is selected to be 100kΩ. RUVLOB is calculated using Equation 25.
RUVLOB is selected to be 9.67kΩ.