RS, the inductor must be selected according to three parameters; calculated inductance value (LM), RMS inductor current at the minimum supply voltage and the peak inductor current limit (ILPEAK_LIMIT) set by the current sense resistor (RS).
- The inductance value is selected to be 2.2 µH. This is a standard value that is produced by most magnetic vendors.
- The RMS current of the inductor can be estimated by calculating the average inductor current (ILAVG) and is approximately equal to the average supply current. The average inductor current is estimated to be 16 A when VSUPPLY = 2.5 V. The inductor RMS current rating should be higher than calculated average inductor current and keep the inductor temperature rise to a reasonable level based on the application.
- The saturation current rating of the inductor should be larger than the calculated ILPEAK_LIMIT value, 25 A. If the inductor becomes saturated, proper operation of the regulator is not ensured.
For this design example, the inductor is selected to have an inductance value of 2.2 µH, 40°C component temperature rise at an RMS of 20 A, and a saturation current limit of 32 A.