SNVA951 November 2020
A thermocouple (TC) can be used to measure the
regulator case temperature as well. This method is more complicated and time
consuming than using a camera. The TC must be much smaller than the package you are
probing and needs to make good thermal contact. If the TC is too large it will act
as a heatsink and lower the actual temperature of the package. You also need to
position the probe as close as possible to the die within the package. Equation 6 is then used to estimate the junction temperature, with the TC
measurement in place of
Tcamera. The TC can
also be placed on the PCB to estimate its temperature. The ΨJB parameter
can then be used to estimate junction temperature from the board temperature, but
this method is not as accurate as using the top case temperature. See Semiconductor and IC Package Thermal Metrics Application Report,
for more details.