SNVA951 November 2020 LM61460-Q1 , LM63615-Q1 , LM63625-Q1 , LM63635-Q1 , LMR33620-Q1 , LMR33630-Q1
The goal of thermal management is to keep the maximum junction temperature of the device at or below a safe value. This safe value is stated in the data sheet under the "Absolute Maximum" specification section as shown in the example of Figure 2-1.
This will usually be 125°C or 150°C for an automotive qualified device and is called TJ-max. A good thermal design will keep the converter temperature below this value under all operating conditions.