SNVA951 November 2020 LM61460-Q1 , LM63615-Q1 , LM63625-Q1 , LM63635-Q1 , LMR33620-Q1 , LMR33630-Q1
The most accurate way to determine thermal performance is with one of the many finite-element type simulators designed for thermal analysis. These tools are rather complicated to use correctly and require detailed information about the PCB and the device package. However, many large companies will have these tools, and perhaps an entire group that is dedicated to performing this type of analysis. This method should be taken advantage of, if it is available.