SNVA951 November   2020 LM61460-Q1 , LM63615-Q1 , LM63625-Q1 , LM63635-Q1 , LMR33620-Q1 , LMR33630-Q1

 

  1.   Trademarks
  2. Introduction
  3. The Goal of Thermal Management
  4. Junction Temperature Calculation
    1. 3.1 Regulator Junction Temperature (TJ)
    2. 3.2 Ambient Temperature (TA)
    3. 3.3 Power Dissipation (PD)
    4. 3.4 Thermal Resistance (θJA)
      1. 3.4.1 Thermal Metrics
  5. Package Type
  6. PCB Copper Heat Sink
  7. PCB Layout Tips
  8. Estimating and Measuring θJA
    1. 7.1 Simple Guideline
    2. 7.2 Data Sheet Curves
    3. 7.3 Simplified Heat Flow Spreadsheet
    4. 7.4 Online Database
    5. 7.5 Thermal Simulators
  9. Measuring Thermal Performance
    1. 8.1 Thermal Camera
    2. 8.2 Thermocouple
    3. 8.3 Internal Diode
  10. Thermal Design Example
  11. 10Conclusion
  12. 11References

Thermal Metrics

Most data sheets include a value for θJA, along with other information, in the thermal characteristics table. Figure 3-1 shows an example from the automotive qualified LM636x5-Q1 3.5-V to 36-V, 1.5-A, and 2.5-A Automotive Step-down Voltage Converter Data Sheet.

GUID-685C6E36-1DDC-42B4-A460-EDD527AD381E-low.gifFigure 3-1 Typical Thermal Metrics From Device Data Sheet

The value of θJA (or RθJA) given in this table is taken under very specific conditions, that do not necessarily apply to the real application. Typically, the value of θJA will be quite a bit larger than what can be achieved with proper PCB layout. Therefore the table value cannot be used for design purposes; its main use is in comparing between different regulators and different packages. As will be shown, the other metrics in the table can be very helpful. For packages with a Die Attach Paddle (DAP) the value of θJC (or RθJC(bott)) for the bottom of the device is also important. Equation 4 shows how to use this parameter.

Equation 4.
GUID-20201105-CA0I-02MF-2HXG-X7X7V42J6PWV-low.gif

In this equation, θSA is the thermal resistance from the heat sink to the ambient air. Usually, the value of θSA is not known and θJA is the true value of interest (Equation 1). However, some calculator tools require θJC when estimating the overall thermal performance. Also, a smaller value of θJC, will help to reduce the overall θJA.

You will notice in the table that there are those metrics termed as "thermal resistance" and those termed as "thermal parameters". The thermal resistance values are defined and measured assuming that all of the power flows in the path indicated by the metric name. As an example, with θJC (or RθJC(bott)) it is assumed that all the power is flowing from the junction to the bottom DAP. These metrics are most important when designing the thermal management of the overall system from the junction to the ambient environment. Thermal parameters are defined and measured assuming that only some of the power is flowing in the path indicated by the metric name. As an example, the parameter ΨJT is used to calculate the junction temperature by measuring the top case temperature with a thermocouple or thermal camera. This calculation is discussed in Section 8.1. Essentially the "Ψ" parameters are used when evaluating and testing the system based on measurements. The "θ" resistances are used when designing or calculating the thermal performance of the system. Suppose a heatsink is used on the top of the package, rather than using the PCB through the bottom DAP connection. A safe assumption would be that most, if not all, of the heat is going through the top heatsink. In this case use the resistance, RθJC(top), rather than the ΨJT parameter to calculate the overall performance. Even though both the metrics indicate heat flow from "junction" to "top", the correct value to use would be the
RθJC(top). The parameter ΨJB can also be useful. A measurement of the board temperature, TB, could be used to estimate TJ using Equation 6. See Semiconductor and IC Package Thermal Metrics to get a much more detailed explanation of thermal metrics and how they are measured and used.