SNVA964 June 2020 LP8866-Q1
In this section we’ll look at the effects of several different techniques and measures to see how they impact the EMI performance of this design. Conducted emissions (current probe method) and radiated emissions measurements are performed. In this case, the current probe method is used to measure conducted emissions on the input power supply wire harness. It measures the common mode current on the power lines which is closely correlated to the radiated emissions from the wires. In this case, the conducted emission measurement result is well correlated to the radiated emission measurement result in the frequency range of 30 MHz to 300 MHz, so the conducted/radiated EMI comparisons are shown together.