SNVAA65 March 2023 LM63610-Q1 , LM63615-Q1 , LM63625-Q1 , LM63635-Q1
For the standard buck converter, the inductor is connected to VOUT and the switch pin (SW) of the LM63615-Q1. To change to an inverting buck-boost topology, the VOUT and ground nodes of the circuit must be reversed. With the nodes reversed, the LM63615-Q1 can now invert the output voltage from the input voltage.
To change an LM63615-Q1 buck converter to an inverting buck-boost, reassign the buck converter VOUT to system ground, and the old buck system ground to -VOUT. The input capacitor will need to be reconnected to the new system ground, and a new bypass capacitor, CIO, is needed between VIN and -VOUT. The positive input and the feedback resistors will remain the same as in the buck converter. To adjust the output of the inverting buck-boost, calculate the feedback resistor values as if it was a buck converter. For further reading on the inverting buck-boost topology, refer to the Working with Inverting Buck-Boost Converters application note. The schematics in #ID-B6C9A22A-CA23-4644-FA3C-C4FA7281CD60 show the changes that have to be made when configuring the LM63615-Q1 buck converter as an inverting buck-boost converter.