SNVAA70 june 2023 LM5176 , LM5176-Q1
Due to the direction change in this application, the power supply needs to have the capacity to sink and source current. The buck-boost regulator is a good choice in this application. Most buck-boost modules and converters are limited in sink current; therefore, the buck-boost controller is selected in this note. LM5176 is a wide-input voltage four-switch buck-boost controller device with integrated drivers for N-channel MOSFETs. LM5176 can automatically transfer between the buck and boost mode. When Vin equals Vout, the device also provides a low ripple output voltage.
In this design, the LM5176 is supplied by a regulated voltage rail of 15 V. The TEC is connected between the Vin and Vout pin of the LM5176. The output voltage can be varied from 5 V to 25 V by adjusting the Vctrl in the microcontroller. Since Vin is fixed, the voltage applied on the TEC can be changed from -10 V to 10 V, which can regulate the current of TEC.