SNVAA71 October 2023 TPSM63610
By changing the buck configuration into an IBB configuration, the average inductor current is affected. The output current capability in the IBB topology is less than the buck configuration. The maximum achievable current is calculated by the following:
The operating duty cycle for an inverting buck-boost converter can be found with Equation 2.
VOUT in Equation 2 is represented with a negative value.
The efficiency term in Equation 2 adjusts the equations in this section for power conversion losses and yields a more accurate maximum output current result. A conservative value efficiency of 70% is used for calculating the duty cycle. Use Equation 1 and Equation 2 to calculate the recommended maximum output current. For example a 24-V input voltage, –5-V output voltage application using the TPSM63610 power module results in a maximum output current of 6.2 A.
VOUT (V) | VIN (V) | IL_max | D | IOUT (A) |
---|---|---|---|---|
-1.2 | 24 | 8 | 0.063 | 7.5 |
-1.8 | 24 | 8 | 0.093 | 7.3 |
-2.5 | 24 | 8 | 0.126 | 7.0 |
-3.3 | 24 | 8 | 0.161 | 6.7 |
-5 | 24 | 8 | 0.230 | 6.2 |
VOUT (V) | VIN (V) | IL_max | D | IOUT (A) |
---|---|---|---|---|
-1.2 | 24 | 6 | 0.063 | 5.6 |
-1.8 | 24 | 6 | 0.093 | 5.4 |
-2.5 | 24 | 6 | 0.126 | 5.2 |
-3.3 | 24 | 6 | 0.161 | 5.0 |
-5 | 24 | 6 | 0.230 | 4.6 |