SNVAA82 august 2023 LMR38020
The secondary output diode must block the maximum input voltage reflected to the secondary side of the transformer. Choose a diode of the voltage rating satisfying Equation 14. And the current rating of the diode must be larger than the secondary output current. Schottky diodes are the best choices. Ultra-fast recovery diodes can also be used. The forward voltage drop of the diode is also an important factor to consider for it limits the maximum secondary output voltage.