SNVAA82 august 2023 LMR38020
Figure 3-1 shows the typical steady state waveforms of a Fly-Buck™ converter in which Vpri is the primary voltage across the coupled inductor, im is the magnetizing current, im and isec are primary side current and secondary side current.
The operation of the Fly-Buck™ converter basically has two modes: TON and TOFF.
TON Mode
This mode is the same as traditional synchronous buck converter when the main switch(HS) is ON. The voltage stress of the low-side (LS) switch is the input voltage(VIN). The magnetizing inductance, Lm is charged by the input voltage minus the primary output voltage as in the regular buck converter. The secondary winding current remains zero for the diode D2 is reverse biased according to the winding polarity configuration, and D2 sees voltage stress of (N2/N1)×(VIN-VOUT1)+VOUT2. The isolated output capacitor COUT2 is supplying the load current.
TOFF Mode
In this mode LS is ON and HS is OFF. Vpri becomes negative, forward biasing D2 to force a secondary current to flow to transfer part of the stored energy in the coupled inductor to the secondary output capacitor, COUT2 and the load, RLoad2.
Unlike the buck converter, ipri in Fly-buck decreases at a faster rate, owing to supplying current to both loads, IOUT1 and IOUT2.
The secondary current waveform is determined by the load, leakage inductance, and output capacitance. The current direction of ipri at the end of one switching cycle (positive or negative) depends on factors including the current ratio of IOUT2: IOUT1 and current ripple.
The primary output voltage is the same as a buck converter and is given by Equation 1.
The secondary output voltage is given by Equation 2.
where