SNVAA84 October 2023 LMR36506
Loop stability is an important factor in the system. The guideline for a stable design is a desired phase margin of at least 45°. The loop stability is measured for the designed fly-buck-boost design with the following conditions:
Gain and phase margin plots measured for the previous conditions are shown in Figure 3-12 with the cross-over frequency of approximately 20 kHz and phase margin in the range of 60°. These test points make sure that the design is stable.