SNVAA88 December   2023 LM51581-Q1 , TPS1H000-Q1 , TPS92642-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2System Description
    1. 2.1 Dual Cable Concept
    2. 2.2 Single Cable Concept
  6. 3Camera Module Design with Single Coaxial Cable Connection
    1. 3.1 Power-Over-Coax Filter
    2. 3.2 Boost Converter
    3. 3.3 High-Side Switch
    4. 3.4 Buffer Capacitor
    5. 3.5 LED Driver
    6. 3.6 Serializer
    7. 3.7 Design Steps
  7. 4Test Results
    1. 4.1 LED and PoC Voltage Waveforms
    2. 4.2 Margin Analysis Program Result
    3. 4.3 Differential Supply Noise Level
    4. 4.4 Test Cases
  8. 5Summary
  9. 6References

Design Steps

The following equations provide a guideline to calculate the required parameters for the design configuration.

The first step is to calculate the required energy which needs to be stored in the buffer capacitor for a single LED pulse with Equation 1.

Equation 1. ELED=VF(MAX)×ILED×N×tONη

where

  • VF(MAX) is the maximum forward voltage of one IR LED
  • ILED is the desired peak LED current
  • N is the number of LEDs connected in series
  • tON is the desired LED current pulse on-time
  • η is the estimated efficiency of the LED driver

In the next step, the required high-side switch current limit can be calculated with Equation 2.

Equation 2. ILIM(MIN)=ELEDVBoost×tOFF

where

  • VBoost is the configured output voltage of the boost converter stage
  • toff specificies the time for recharging the buffer capacitor and can be selected depending on the LED pulse frequency and on-time

The calculated value represents the minimum recharge current which is required to fully recharge the buffer capacitor before the next LED pulse occurs.

Once an appropiate recharge current has been selected, the resulting input current which flows over the coaxial cable and PoC filter inductors can be determined with Equation 3.

Equation 3. IPoC=ILIM×VBoostVPoC×1η+I2

where

  • ILIM is the selected recharge current limit
  • VPoC is the voltage on the coaxial cable
  • η is the estimated efficiency of the boost converter
  • ΔI is the peak-to-peak inductor ripple current, which is typically 20 - 40 % of the output current

In the last step, the required buffer capacitor size can be calculated with Equation 4.

Equation 4. CBUF(MIN)=2×ELED-ILIM(MIN)×VBoostVBoost2-VBUF(MIN)2

VBUF(MIN) represents the minimum voltage level in the buffer capacitor at the end of the discharge cycle. The minimum voltage level must be greater than the maximum expected output voltage of the LED driver.