SNVSC75A April 2023 – July 2024 LM5171-Q1
ADVANCE INFORMATION
A sequential write operation is an extension of the single write protocol and shown in Figure 6-39 . If the Controller does not send a stop condition after the device has issued an ACK, the device auto increments the register address by one and the Controller can write to the next register.