SNVU543A November 2016 – December 2016 LM5170 , LM5170-Q1
Power Supplies: HV-PS should be capable of 80V/20A, and LV-PS 40V/80A. To operate 2 EVMs in 4 phase configuration, the HV-PS and LV-PS capabilities should be doubled. Bench power supplies to generate UVLO, ISETA, DIR, and EN1 and EN2 signals should be capable of 5V/0.1A.
Electronic Loads: The HV-E-Load should be capable of 80V/20A, and LV-E-Load 40V/80A. To operate 2 EVMs in 4 phase configuration, the E-Loads’ capabilities should be doubled.
Meters: Because most current meters are rated only to 10 A, shunts are recommended to measure the current using a DVM.
Oscilloscope: An oscilloscope and 10x probes with at least 20-MHz bandwidth is required. Current probe capable of 50 A is required to monitor the inductor current via a wire loop inserted to the non-switching side of the inductor.