SNVU699 October 2020
The REF70 VREF is the output of the REF70 when the OUTF and OUTS are shorted together. OUTF and OUTS refer to the force and sense configuration of the REF70 reference buffer. The benefit of having force and sense connection is to reduce the IR loss from long trace wires at high currents. In the normal active configuration, the OUTF and OUTS are shorted together. In the REF70EVM this is done by the R1 and R2 which are 0 Ohm resistors. If R1 or R2 is removed, OUTF and OUTS must be connected in a loop by the headers J3/J7 or externally for proper operation. If the OUTF and OUTS are not connected together in a loop then the device will not operate the correct voltage.