SNVU751 October   2020 LP875761-Q1

 

  1. 1Trademarks
  2. 2Overview
  3. 3Quick Setup Guide
    1. 3.1 Installing/Opening the Software
    2.     5
    3. 3.2 Power Supply Setup
    4. 3.3 Notes on Efficiency Measurement Procedure
  4. 4GUI Overview
    1. 4.1 Main Tab
    2. 4.2 Other Tabs and Menus
    3. 4.3 Console
  5. 5Bill of Materials
  6. 6Board Layout
  7. 7LP875761Q1EVM Schematics
  8. 8Revision History

Installing/Opening the Software

The EVM software is controlled through a graphical user interface (GUI). The software communicates with the EVM through an available USB port. The minimum hardware requirements for the EVM software are:

  • IBM PC-compatible computer running a Microsoft Windows XP® or newer operating system
  • Available USB port
  • Mouse

Software installation

  1. Open the LP8757_installer.exe.
  2. Installer prompts to accept the license agreement (see Figure 3-1).
  3. Installer prompts to choose which features of LP8757 Installer you want to install (see Figure 3-2).
  4. Installer prompts to select Destination Folder (see Figure 3-3).
  5. Press Install and the installation starts.
  6. Installer prompts when installation is complete (see Figure 3-4).

Open the LP8757 GUI. Connect the EVM to the PC with the USB cable.

  1. With the power supply disconnected from the unit under test (UUT), open LP8757.exe located in the directory selected during installation.
  2. On the Evaluation SW window bottom right corner you should see text Hardware connected. Refer to Figure 3-5.