HotRod™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.
The LM62460-Q1 is an easy-to-use synchronous step-down DC-DC converter capable of driving up to 6 A of load current from a supply voltage ranging from 3 V to 36 V. The LM62460-Q1 provides exceptional efficiency and output accuracy in a very small solution size. The LM62460-Q1 implements peak-current-mode control. Additional features such as adjustable/synchronizable switching frequency, pin selectable dual-random spread spectrum (DRSS), true slew rate control, FPWM/AUTO selection, power-good/RESET flag, and precision enable provide both flexible and easy-to-use solutions for a wide range of applications. Automatic frequency foldback (AUTO mode) at light load and optional external bias improve efficiency over the entire load range. The device family requires few external components and has a pinout designed for simple PCB layout with excellent EMI and thermal performance. Protection features include thermal shutdown, input undervoltage lockout, cycle-by-cycle current limiting, and hiccup short-circuit protection. The LM62460-Q1 is pin-to-pin compatible with LM61480-Q1 (8-A converter) and LM61495-Q1 (10-A converter) for easy current scaling.
The pin configuration of the LM62460-Q1 is shown in Figure 1-1.
This section describes the connectors and the test points on the EVM.
VIN_EMI terminal connects to the input capacitors and the VIN pins of the LM62460-Q1 through an input EMI filter. Connect the supply voltage (battery, bench-top supply, or other supply) between VIN_EMI and GND_EMI connectors. The voltage range should be higher than 3.5 V for the device to start up, and above 3V to continue operation. VIN higher than 6 V provides regulated 5 V output voltage. VIN should be no higher than 36 V to avoid damaging the device. The current limit on the supply must be high enough to provide the needed supply current, otherwise the supply voltage may not maintain the desired voltage. The supply voltage should be connected to the board with short, thick wires to handle the pulsing input current.
This is the current return path for the supply connected to VIN_EMI.
VOUT terminal connects to the power inductor and the output capacitors. Connect the loading device between VOUT and GND connectors on J2 to load the converter output. Connect the loading device to the board with short, thick wires to handle the large DC output current.
This is the current return path for the output voltage connected to VOUT.
The input filter consists of a ferrite bead, filter inductor, and filter capacitors, located on the bottom side of the PCB. The output of the filter is connected to the VIN net, which is connected to the VIN pins of the LM62460-Q1 and the input capacitors.
Conducted EMI arises from the normal operation of switching circuits. The ON and OFF actions of the power switches generate large discontinuous currents. The discontinuous currents are present at the input side of buck converters. Voltage ripple generated by discontinuous currents can be conducted to the voltage supply of the buck converter via physical contact of the conductors. Without control, excessive input voltage ripple can compromise operation of other devices connected to the source. The input filter helps to smooth out the voltage perturbations leading to the source.
Place the shunt connecting FB and 5V to set VOUT = 5V. Place the shunt connecting FB and 3.3V to set VOUT = 3.3V.
The LM62460RPHEVM schematic is shown in Figure 4-1.