The test points on the board can be used to
connect to the input of a power supply and output load for the EVM. See Figure 1-1 for typical test setup. The functions of the test point connections are:
Vin_EMI — Input supply to EVM including an EMI filter. Connect to a
suitable input supply. Connect at this point for EMI tests.
GND_EMI — Ground connection for the input supply
Vin — Input supply to the IC. Can be connected to a digital multimeter to
measure the input voltage after EMI filter.
VOUT — Output voltage test point of EVM. Can be connected to a desired
load.
GND — Ground test points
PG — This test point is connected to the PGOOD pin from the IC. Can be
tied to an external supply through a pullup resistor or left open.
SYNC — In a MODE/SYNC trim part, this test point is connected to
the SYNC pin of the IC. This test point can also be connected to an external
clock to synchronize the IC. Make sure the RT resistor is not installed when
applying a synchronous clock input. If RMOD is installed, JMODE/SYNC jumper must
not short pin 2 to either adjacent pins while applying a synchronous clock
input. For evaluating RT trim parts, see the JMODE/SYNC jumper
description in Section 1.2.
Vcc — This test point is
connected to the Vcc pin of the IC.
AGND— This test point represents the analog ground test point and is
connected to the ground plane.