SNVU843A April 2023 – November 2023
Power Supplies: HV-PS needs to be capable of 80 V/20 A, and LV-PS 40 V/80 A. To operate 2 EVMs in 4 phase configuration, double the capabilities of the HV-PS and LV-PS. Bench power supplies to generate UVLO, ISETA, DIR, and EN1 and EN2 signals need to be capable of 5 V/0.1A.
Electronic Loads: The HV-E-Load needs to be capable of 80 V/20 A, and LV-E-Load 40 V/80 A. To operate 2 EVMs in 4 phase configuration, double the capability of the E-Load.
Meters: Because most current meters are rated only to 10 A, shunts are recommended to measure the current using a DVM.
Oscilloscope: An oscilloscope and 10x probes with at least 20-MHz bandwidth is required. Current probe capable of 50 A is required to monitor the inductor current via a wire loop inserted to the non-switching side of the inductor.