SNVU844 may 2023
Figure 3-1 depicts the high level flow in the sample code.
The FC_settings.h file can automatically be generated by the Registers Map Generation Tool mentioned in Section 2. Not all register settings are coming from this file. The number of scan lines (field SCAN_NUM in register FC0) and the number of cascaded devices (field CHIP_NUM in register FC0) are coming from the file system_info.h. This file is described in more detail in Section 3.3.
The flow diagram also shows the files frames.c and frames.h which contain the 2 frames used during the animation mode. It is outside the scope of this document to explain how these frames are generated.