SNVU868A September 2023 – April 2024
The LP5813/12 Evaluation Module showcases all the features of the LP5813 and LP5812 4 × 3 matrix RGB LED driver with autonomous control. The difference between 2 devices is with or without synchronous boost function. Both LP5813 and LP5812 are placed on 1 board, please select the device which is needed to be evaluated by USB2ANY connector and jumper setting. And please select the right EVM version according to different package (WSON/WCSP). The graphical user interface or GUI called LP581x GUI is used to interface with USB to the EVM by the USB2ANY interface adapter.