SNVU870A June 2023 – October 2023
In the default jumper setting, the board can be evaluated by USB power directly and does not need an external power supply. Setup connection is demonstrated in Figure 2-1. The setup procedure is as follows:
Figure 2-2 shows the default jumper settings.
If maximum current is set above 20 mA, then an external VLED supply is recommended during evaluation since the USB can only provide around 400-mA current. The setup procedure is as follows: