SNVU888 March 2024
The LP5811/10 evaluation module showcases all the features of the LP5811 and LP5810 4 channels RGB LED driver with autonomous control. The difference between the two devices is dependent on whether there is a synchronous boost function. The evaluation module includes four ICs on 1 PCB board: LP5811WCSP, LP5811WSON, LP5810WCSP, and LP5810WSON. Select the device by jumper setting and I2C target address. The graphical user interface (GUI) is called LP581XEVM-GUI. The GUI is used to interface with USB to the EVM by the USB2ANY interface adapter.