SNVU888 March 2024
Multiple devices can be evaluated at same time.
If LP5810A is under test, then use I2C target address 0x14 and setup the jumper with "A". (J18, J1, J2, J3, J43)
If LP5811B is under test, then use I2C target address 0x15 and setup the jumper with "B". (J18, J16, J21, J23, J26, J43)
If LP5810C is under test, then use I2C target address 0x16 and setup the jumper with "C". (J18, J15, J8, J10, J43)
If LP5811D is under test, then use I2C target address 0x17 and setup the jumper with "D". (J18, J17, J35, J36, J39, J43)
On the default jumper setting, users can evaluate LP5811D under the conditions below:
Figure 2-2 shows the default jumper settings.
Users can configure the EVM by different jumper settings. The sections below illustrate the functions of the jumpers.
Jumper Number | Upper Pin | Center Pin 1 | Center Pin 2 | Lower Pin |
---|---|---|---|---|
J18 | VCC_D | VCC_C | VCC_A | VCC_B |
VCC | ||||
J19 | VCC_EXT | VCC | VCC | 3V3_U2A |
VCC: Power supply can be connected to the device that is under evaluation.
VCC_X: The power supply for device with "X" part number. For example, VCC_A is the power supply for LP5810A.
VCC_EXT: External power supply.
3V3_U2A: Power supply from USB2ANY interface adapter.
Jumper Number | Left Pin | Right Pin |
---|---|---|
J40 | 3V3_Pull_Up | 3V3_U2A |
J41 | I2C_SCL | SCL_U2A |
J42 | I2C_SDA | SCL_SDA |
3V3_Pull_Up: 3.3V pull up for I2C signal, connected to SDA/SCL by 4.7kohm resistor.
I2C_SCL/SDA: I2C signal, connected to all devices on the board.
SCL/SDA_U2A: I2C signal from USB2ANY interface adapter.
3V3_U2A: Power supply from USB2ANY interface adapter.
Jumper number | Upper Pin | Center Pin | Lower Pin |
---|---|---|---|
J14 | VCC_A | - | VIN_A |
J15 | VIN_C | - | VCC_C |
J16 | VIN_B | VCC_B | VOUT_B |
J17 | VOUT_D | VCC_D | VIN_D |
VCC_X: Power supply for device with "X" part number. For example, VCC_A is the power supply for LP5810A.
VIN_X: Power supply for LP5810 or Input voltage for LP5811 boost module.
VOUT_X: Output voltage for LP5811 boost module or power supply for LP5811 when working on linear mode (boost disabled).
Jumper Number | Left Pin | Center Pin | Right Pin |
---|---|---|---|
J35 | L | EN_D | H |
J21 | L | EN_B | H |
EN_D/B: Enable pin for LP5811B/D: pull high to enable boost function, pull low to disable the boost.
L: Connect to GND.
H: Connect to VIN_B/D.
Jumper Number | Upper Pin | Center Pin 1 | Center Pin 2 | Lower Pin |
---|---|---|---|---|
J10/J39 | D3_C/D | D2_C/D | D1_C/D | D0_C/D |
OUT3_C/D | OUT2_C/D | OUT1_C/D | OUT0_C/D | |
J3/J26 | D0_A/B | D1_A/B | D2_A/B | D3_A/B |
OUT0_A/B | OUT1_A/B | OUT2_A/B | OUT3_A/B |
DX_Y: Connect to LEDX for device Y version. For example, D0_A is connected to LED0 for LP5810A.
OUTX_Y: Connect to the output channel X of device Y. For example, OUT0_A is connected to output channel 0(OUT0) of LP5810A.
Jumper Number | VLED |
---|---|
J43 | VOUT_D |
VIN_C | |
VLED_EXT | |
VLED_EXT | |
VIN_A | |
VOUT_B |
The LED supply voltage VLED can be provided by both LED driver power supply(VOUT_B/D, VIN_A/C) and external power supply (VLED_EXT).
Jumper Name | Left Pin | Right Pin |
---|---|---|
J2/J8 | GND | SYNCA/C |
J23/J36 | SYNCB/D | GND |
Jumper Number | Left Pin | Center Pin 1 | Center Pin 2 | Right Pin |
---|---|---|---|---|
J9 | SYNC_A | SYNC_C | SYNC_D | SYNC_B |
SYNC_COM |
The SYNC pin can be used to synchronize the lighting effects among multiple devices. When this function is not used, connect to GND.
If multiple device need to be tested together, then the SYNC pin is useful for synchronizing the devices. At that time, connect the SYNC_X of the devices under tested to the SYNC_COM, which is the common point for SYNC signal.
After the multiple SYNC signals are connected together, make sure one of the LED drivers is configured the SYNC pin to output, and other devices are configured as SYNC input. Otherwise, an external clock is needed for the SYNC_COM.