The EVM can be powered by USB2ANY directly when J19 is connected to 3V3_U2A. If the input current needs to be measured, then an external VIN/VCC supply is recommended during evaluation.
- Connect the USB2ANY to the LP5811-10EVM using the ribbon cable.
- Connect a 1.8-5.5V external power supply to the VCC_EXT terminal (TP4) and connect the switching jumper (J19) to VCC_EXT.
- If the user wants to evaluate LP5811 but disable the boost function, then provide power supply from Vout instead of VIN and connect the EN_B/D (J35/J21) to L.
- Plug the USB cable into the USB port on the computer.
See the external power supply connection in Figure 2-3.