SPMA041G January   2012  – October 2015 TM4C1230C3PM , TM4C1230C3PM , TM4C1230D5PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PM , TM4C1231H6PZ , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232C3PM , TM4C1232D5PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PM , TM4C1233H6PZ , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236D5PM , TM4C1236E6PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PM , TM4C1237H6PZ , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AE6PM , TM4C123AH6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PM , TM4C123BH6PZ , TM4C123BH6PZ , TM4C123BH6ZRB , TM4C123BH6ZRB , TM4C123FE6PM , TM4C123FE6PM , TM4C123FH6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C123GH6ZRB , TM4C123GH6ZXR , TM4C123GH6ZXR , TM4C1290NCPDT , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TM4C129XNCZAD

 

  1.   Using the CMSIS DSP Library in Code Composer Studio for TM4C MCUs
    1.     Trademarks
    2. 1 Introduction
    3. 2 CMSIS DSP Library
    4. 3 Building the DSP Library in Code Composer Studio v6.1
      1. 3.1 Adding the CCS-Required Header Files to the DSP Libraries
      2. 3.2 Creating the dsplib Project
      3. 3.3 Adding the dsplib Source Code
      4. 3.4 Editing the dsplib Project Settings
      5. 3.5 Building the dsplib Source Code
    5. 4 ARM Example Projects
      1. 4.1 Creating the ARM Example Projects
      2. 4.2 Adding the Example Source Code
      3. 4.3 Editing the Example Project Settings
      4. 4.4 Building, Running, and Verifying the Project
      5. 4.5 Source Code Modifications
    6. 5 Conclusion
    7. 6 References
  2.   Revision History

Creating the dsplib Project

Before building the DSP library in Code Composer Studio, you must create a project for the library. You can build a project by completing the following steps:

  1. Launch CCSv6.1 and select an empty workspace.
  2. Select File → New → CCS Project. The New Code Composer Studio Project window will be displayed.
  3. Select Target as TM4C Series and then use the drop down menu to select TM4C1294NCPDT. Select the Connection as Stellaris In-Circuit Debug Interface (see Figure 1).
  4. In the Project name, type dsplib-cm4f and keep the check box ticked for the Use default location.
  5. In Advanced settings, select:
    • Output type: Static Library
    • Output format: eabi (ELF)
    • Device endianness: little
  6. In Project templates and examples (see Figure 2), select Empty Project.
  7. Click Finish to create the project. The dsplib-cm4f project appears in the Project Explorer.
Pic1.pngFigure 1. Creating the dsplib Project
Pic2.pngFigure 2. Creating the dsplib Project