SPMU373A March   2021  – August 2022 TM4C1230C3PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PZ , TM4C123BH6ZRB , TM4C123FE6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C123GH6ZXR , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD

 

  1.   Read This First
    1.     About This Manual
    2.     Glossary
    3.     Related Documentation From Texas Instruments
    4.     Support Resources
    5.     Trademarks
  2. 1Introduction to TivaWare SDK
    1. 1.1 TivaWare SDK Folder Breakdown
  3. 2TivaWare Example Projects
    1. 2.1 TivaWare Development Board Examples
    2. 2.2 TivaWare Peripheral Examples
    3. 2.3 How to Import an Example Project into CCS
  4. 3Linking Files and Libraries into a TivaWare Project in Code Composer Studio
    1. 3.1 Linking Files in CCS
    2. 3.2 Linking Libraries in CCS
  5. 4How to Debug a TivaWare Library
    1. 4.1 How to Direct Code Composer Studio to a Source File
    2. 4.2 How to Rebuild TivaWare Libraries
  6. 5How to Add TivaWare to an Existing CCS Project
    1. 5.1 Path Variables
    2. 5.2 Include Paths
    3. 5.3 Predefined Variables
    4. 5.4 Library Linking
  7. 6TivaWare Boot Loader
    1. 6.1 Modifying a TivaWare Project for Boot Loading in Code Composer Studio
    2. 6.2 How to Boot Load with LM Flash Programmer
  8. 7Software Best Practices
    1. 7.1 Stack / Heap Settings and Stack Overflow
    2. 7.2 Interrupt Service Routines
      1. 7.2.1 Best Practices
      2. 7.2.2 TivaWare Vector Tables and IntDefaultHandler
    3. 7.3 TivaWare Hardware Header Files
    4. 7.4 ROM and MAP TivaWare Prefixes
  9. 8TM4C Resources
  10. 9Revision History

Predefined Variables

The next step is to add in a predefined symbol into the project. Predefined symbols are used by TivaWare files including in DriverLib to select code blocks based on the TM4C MCU family used. To add a symbol first go to CCS Project Properties and then navigate to Build → ARM Compiler → Predefined Symbols. There should already be at least one symbol defined for the TM4C microcontroller being used such as the PART_TM4C123GH6PM shown in Figure 6-3. If for some reason that is not present, it must be added as well. The part number that should be used after ‘PART_’ would be the device that was chosen in the ‘General’ section of the Project Properties.

To add a new symbol, click the ‘Add…’ button and type in the value into the box that pops up. The symbol that needs to be added depends on the MCU family used. If a TM4C123x device is used, then add TARGET_IS_TM4C123_RB1. If a TM4C129x device is used, then add TARGET_IS_TM4C129_RA2. Click ‘OK’ to add the new symbol.

GUID-20201218-CA0I-G8J9-CJT9-GT4J5GV09KVD-low.jpg Figure 5-3 Predefined Symbols Menu in CCS Project Properties