SPMU373A March 2021 – August 2022 TM4C1230C3PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PZ , TM4C123BH6ZRB , TM4C123FE6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C123GH6ZXR , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD
Code Composer Studio has an easy-to-use import feature that can be found under Project → Import CCS Projects. To import any TivaWare project click the ‘Browse’ button with the ‘Select search-directory’ option. This feature will look for all CCS projects in a provided directory. Due to the number of examples projects offered within the TivaWare SDK, it is strongly encouraged to navigate to at least a specific board level if not to the exact project desired. Figure 3-1 shows the options when navigating to examples\boards\ek-tm4c123gxl.
It is possible to import multiple projects at once. Simply scroll through the list and select all projects that should be imported and click ‘Finish’. All TivaWare example projects will automatically be copied into the workspace as a new project so the original project will be left untouched and can be re-imported at any time.
Because the projects are copied into the workspace, if a previously imported project is removed from the workspace in CCS but not deleted from the file system then an error may indicate that the project still exists in the workspace. In this situation, either re-import the project back into CCS from the workspace directory or delete the project folder from the workspace directory and try to import the project from the TivaWare directory again.