SPMU373A March   2021  – August 2022 TM4C1230C3PM , TM4C1230D5PM , TM4C1230E6PM , TM4C1230H6PM , TM4C1231C3PM , TM4C1231D5PM , TM4C1231D5PZ , TM4C1231E6PM , TM4C1231E6PZ , TM4C1231H6PGE , TM4C1231H6PM , TM4C1231H6PZ , TM4C1232C3PM , TM4C1232D5PM , TM4C1232E6PM , TM4C1232H6PM , TM4C1233C3PM , TM4C1233D5PM , TM4C1233D5PZ , TM4C1233E6PM , TM4C1233E6PZ , TM4C1233H6PGE , TM4C1233H6PM , TM4C1233H6PZ , TM4C1236D5PM , TM4C1236E6PM , TM4C1236H6PM , TM4C1237D5PM , TM4C1237D5PZ , TM4C1237E6PM , TM4C1237E6PZ , TM4C1237H6PGE , TM4C1237H6PM , TM4C1237H6PZ , TM4C123AE6PM , TM4C123AH6PM , TM4C123BE6PM , TM4C123BE6PZ , TM4C123BH6PGE , TM4C123BH6PM , TM4C123BH6PZ , TM4C123BH6ZRB , TM4C123FE6PM , TM4C123FH6PM , TM4C123GE6PM , TM4C123GE6PZ , TM4C123GH6PGE , TM4C123GH6PM , TM4C123GH6PZ , TM4C123GH6ZRB , TM4C123GH6ZXR , TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD

 

  1.   Read This First
    1.     About This Manual
    2.     Glossary
    3.     Related Documentation From Texas Instruments
    4.     Support Resources
    5.     Trademarks
  2. 1Introduction to TivaWare SDK
    1. 1.1 TivaWare SDK Folder Breakdown
  3. 2TivaWare Example Projects
    1. 2.1 TivaWare Development Board Examples
    2. 2.2 TivaWare Peripheral Examples
    3. 2.3 How to Import an Example Project into CCS
  4. 3Linking Files and Libraries into a TivaWare Project in Code Composer Studio
    1. 3.1 Linking Files in CCS
    2. 3.2 Linking Libraries in CCS
  5. 4How to Debug a TivaWare Library
    1. 4.1 How to Direct Code Composer Studio to a Source File
    2. 4.2 How to Rebuild TivaWare Libraries
  6. 5How to Add TivaWare to an Existing CCS Project
    1. 5.1 Path Variables
    2. 5.2 Include Paths
    3. 5.3 Predefined Variables
    4. 5.4 Library Linking
  7. 6TivaWare Boot Loader
    1. 6.1 Modifying a TivaWare Project for Boot Loading in Code Composer Studio
    2. 6.2 How to Boot Load with LM Flash Programmer
  8. 7Software Best Practices
    1. 7.1 Stack / Heap Settings and Stack Overflow
    2. 7.2 Interrupt Service Routines
      1. 7.2.1 Best Practices
      2. 7.2.2 TivaWare Vector Tables and IntDefaultHandler
    3. 7.3 TivaWare Hardware Header Files
    4. 7.4 ROM and MAP TivaWare Prefixes
  9. 8TM4C Resources
  10. 9Revision History

How to Boot Load with LM Flash Programmer

The TI offered LM Flash Programmer utility tool enables boot loading for TM4C devices over UART, USB, and Ethernet interfaces. In order to use the tool for boot loading, select the Manual Configuration option in the Quick Set section of the Configuration tab (Figure 7-1). After Manual Configuration is selected, then the Interface section can be used to select one of the three boot loading options of Serial (UART), Ethernet, and USB DFU.

GUID-20220825-SS0I-MS3J-D8L5-4RSBJ1HW44SX-low.jpg Figure 6-1 LM Flash Programmer Manual Configuration

 

For the Ethernet boot loader, it is important to ensure the correct Client MAC Address is entered. When using the USB DFU mode, the TM4C microcontroller must be in a state where the USB boot loader is running so that the PC can recognize the USB DFU port. If no devices show up on the list, invoke the USB boot loader on the TM4C microcontroller and then use the refresh button to trigger LM Flash Programmer to search for the USB DFU interface again.

Once the desired interface is setup, move to the Program tab to select the binary file for programming. Browse the local file system to find the .bin file for your project (Figure 7-2). This will always be located in the Debug folder of a CCS project.

GUID-20210210-CA0I-B34H-VP82-LPLKCLXQDM6K-low.jpg Figure 6-2 Browse for .bin File

 

Once the file is selected, set the correct Program Address Offset (Figure 7-3). This will be equal to the APP_START_ADDRESS. Once these steps are completed, press the Program button to trigger the boot loading process and upload the application firmware onto the device.

GUID-20210210-CA0I-X9JX-M8QV-3ZDLXSZ7GW3P-low.jpg Figure 6-3 Set the Program Address Offset Value