SPNA209C January 2015 – January 2020 RM42L432 , RM44L520 , RM44L920 , RM46L430 , RM46L440 , RM46L450 , RM46L830 , RM46L840 , RM46L850 , RM46L852 , RM48L530 , RM48L540 , RM48L730 , RM48L740 , RM48L940 , RM48L950 , RM48L952 , RM57L843 , TMS570LC4357 , TMS570LC4357-EP , TMS570LC4357-SEP , TMS570LS0332 , TMS570LS0432 , TMS570LS0714 , TMS570LS0714-S , TMS570LS0914 , TMS570LS1114 , TMS570LS1115 , TMS570LS1224 , TMS570LS1225 , TMS570LS1227 , TMS570LS2124 , TMS570LS2125 , TMS570LS2134 , TMS570LS2135 , TMS570LS3134 , TMS570LS3135 , TMS570LS3137 , TMS570LS3137-EP
The HALCoGen Compliance Support Package (CSP) was developed to provide documentation, reports and unit test capability to assist customers using HALCoGen generated software to comply with functional safety standards such as IEC 61508 and ISO 26262. HALCoGen-CSP 04.07.01 is available in 10 variants supporting TMS570LC43x, TMS570LS31x_21x, TMS570LS12x_11x, TMS570LS09x_07x, TMS570LS04x_03x, TMS570LC43x, TMS570LS09x_07x, RM57x, RM48x, RM46x, RM44x and RM42x family of devices. Customers can choose and purchase the package for the device family used in their product development.
Hercules is a registered trademark of Texas Instruments.
Windows is a registered trademark of Microsoft Corporation in the United States and other countries.
All other trademarks are the property of their respective owners.
The HALCoGen-CSP features unit level and functional test cases developed by TI and can be run using the included Test Automation Unit (TAU), which utilizes the LDRAUnit from LDRA. The HALCoGen-CSP also provides infrastructure for the customers to add their own test cases using Test XLS template and HALCoGen TAU. For more information, see the HALCoGen-CSP User's Guide.