SPRAB89A September 2011 – March 2014
Floating-point behavior varies by device and by toolchain and is therefore difficult to standardize. The goal of the ABI is to provide a basis for conformance to the C, C99, and C++ standards. Of these C99 is the best-specified with respect to floating-point. Appendix F of the C99 standard defines floating-point behavior of the C language behavior in terms of the IEEE floating-point standard (ISO IEC 60559:1989, previously designated as ANSI/IEEE 754−1985).
The C6000 ABI specifies that the helper functions in this section that operate on floating-point values must conform to the behavior specified by Appendix F of the C99 standard.
C99 allows customization of, and access to, the floating-point behavioral environment though the <fenv.h> header file. For purposes of standardizing the behavior of the helper functions, the ABI specifies them to operate in accordance with a basic default environment, with the following properties:
A toolchain is free to implement more complete floating-point support, using its own library. Users who invoke toolchain-specific floating-point support may be required to link using that toolchain's library (in addition to an ABI-conforming helper function library).