SPRABI1D January 2018 – July 2022 66AK2E05 , 66AK2G12 , 66AK2H06 , 66AK2H12 , 66AK2H14 , 66AK2L06 , AM5K2E02 , AM5K2E04 , SM320C6678-HIREL , TMS320C6652 , TMS320C6654 , TMS320C6655 , TMS320C6657 , TMS320C6670 , TMS320C6671 , TMS320C6672 , TMS320C6674 , TMS320C6678
All data-group signals are point-to-point in the validated topologies. The data-group signals are driven by the KeyStone device on writes and driven by the SDRAM memories during reads. No external resistors are needed on these routes. The receivers in both cases (SDRAMs on writes and KeyStone device on reads) will assert on-die terminations (ODT) at the appropriate times. The following diagrams show the impedances seen on these nets during write and read cycles.
Figure 6-5 shows the impedances seen on the nets during a write cycle. During writes, the output impedance of the KeyStone I device is approximately 45 Ω. It is recommended that the SDRAM be implemented with a 240-Ω RZQ resistor and be configured to present an ODT of RZQ/4 for an effective termination of 40 Ω.
Figure 6-6 shows the impedances seen on the nets during a read cycle. During reads, it is recommended that the SDRAM be configured for an effective drive impedance of RZQ/7 or 34 Ω (assuming RZQ resistor is 240 Ω). The on-die termination (ODT) within the KeyStone I device will have an effective Thevenin impedance of 45 Ω.