SPRABI1D January 2018 – July 2022 66AK2E05 , 66AK2G12 , 66AK2H06 , 66AK2H12 , 66AK2H14 , 66AK2L06 , AM5K2E02 , AM5K2E04 , SM320C6678-HIREL , TMS320C6652 , TMS320C6654 , TMS320C6655 , TMS320C6657 , TMS320C6670 , TMS320C6671 , TMS320C6672 , TMS320C6674 , TMS320C6678
The following subsection describes the two signal termination methods (leveling and non-leveling) used for DDR3 interfaces, specific termination placement, and the impact of incorrect termination schemes and component values. Terminations are placed at the end of the signal path. In the current fly-by architecture, placing the terminations at the last SDRAM improves the overall signal characteristics, which is an improvement over previous DDR2 SDRAM topology.