SPRABI1D January 2018 – July 2022 66AK2E05 , 66AK2G12 , 66AK2H06 , 66AK2H12 , 66AK2H14 , 66AK2L06 , AM5K2E02 , AM5K2E04 , SM320C6678-HIREL , TMS320C6652 , TMS320C6654 , TMS320C6655 , TMS320C6657 , TMS320C6670 , TMS320C6671 , TMS320C6672 , TMS320C6674 , TMS320C6678
The down side to the use of a fly-by topology for DDR3 designs is the induced delay from the DSP DDR3 controller to the SDRAMs. In fact, the delay is different at each SDRAM. Correction or compensation for the different controller-to-DRAM lengths is handled through read and write leveling. Also keep in mind the following: