Tests that are in IEC 61496-5 but
are already covered by results shown in this document are as follows:
- Interference from other radio
sources
- Sensitivity and Stability
- Detection of target with high
RCS
Many of the hardware and system level tests vary based on the system in which the
sensor chip is integrated. Detection of targets with high RCS has been shown throughout
this page and would be redundant for the scope of this document. For more information
regarding interference, see
Interference Mitigation For AWR/IWR Devices.
With the interference mitigation techniques shown within the document, performance will
be robust and reliable even in the presence of other signal emitting devices.