SPRAC03 July 2024 IWR6843
IEC 61496-5:5.4.7.1
When there is a target object inside the detection zone, an interfering target outside the detection zone must not interfere with the target object’s ability to be detected. For this test, Section 4.2.13.4 mentions a 40 m2 CR is used as the interfering target in order to ensure it does not absorb the small 0.17 m2 CR’s visibility. The test calls for the interfering target to be static in one test and dynamic in another. In the dynamic test, the interfering target is moving at the same static residual movement speed as the test target. The interfering corner reflector should not be able to disrupt the detection CR’s visibility, ensuring no disruption via outside objects.
As seen above, the interfering target does not disrupt detection ability of the test target. While the interfering object is dynamic, there is still a clear distinction between it and the target, ensuring that the target is identified as inside the zone.