SPRAC03 July 2024 IWR6843
IEC 61496-5:5.4.6.2
Due to the physics of FMCW millimeter wave radar and interference mitigation techniques, it is highly unlikely for other signals to disrupt the RPD’s signal. However, the standard requests a test in Section 5.4.6 of having four RPDs as interfering targets with identical designs to the RPD under test. The CR must go through static residual movement while having no detection ability deterioration. While the test is underway, the interfering RPDs needs to be power cycled at least 10 times, over the course of two hours. This is to switch up the timings of the chirps.
The resulting point cloud was identical to what it would look like if there were no interfering RPDs at all. This is due to the configured static clutter removal algorithm removing any detections with 0 Doppler. Static clutter removal is not required, but it helps to visualize only moving targets. In addition the detection zone never changed to unoccupied while the target was inside the detection zone.
More details on interference involving multiple RPDs can be found in the document Interference Mitigation For AWR/IWR Devices.