SPRAC21A June 2016 – June 2019 OMAP-L132 , OMAP-L138 , TDA2E , TDA2EG-17 , TDA2HF , TDA2HG , TDA2HV , TDA2LF , TDA2P-ABZ , TDA2P-ACD , TDA2SA , TDA2SG , TDA2SX , TDA3LA , TDA3LX , TDA3MA , TDA3MD , TDA3MV
The interconnect has internal components that can aid in the traffic regulation from a specific initiator to a specific target. The components are called Bandwidth Regulators and Bandwidth limiters. Additionally, the initiator IPs can set their respective MFLAG or MREQPRIORITY signals, which is understood by the interconnect and subsequently DMM/EMIF to give priority to a given initiator.
The default value of the various traffic regulator within the interconnect is set to a default that allows most use case to work without any tweaking. However, if there is any customization needed for a given use case, it is possible by various programmable parameters explained in subsequent sections.