SPRAC71B February 2019 – October 2023
The C28x ABI is based on the ELF object file format. The base specification for ELF is comprised of Chapters 4 and 5 of the larger System V ABI specification (http://www.sco.com/developers/gabi/2003-12-17/contents.html).
The subsections that follow contain C28x processor-specific supplements for Chapter 4 (Object Files) of the specification. Chapter 12 of this document contains processor-specific supplements for Chapter 5 (Program Loading and Dynamic Linking) of the specification.
However, for the C28x ELF format, fields that represent target addresses are native (word-oriented), but fields that represent target sizes are expressed in bytes.